AXIS#.SAFEPARAM.SLS_#.TIMETOVELMONITORING

Description

Indicates the maximum time before starting the velocity monitoring of the Safely Limited Speed (SLS) safety function. If the velocity is not below the limit when this time elapsed then the function is faulted and it activates the configured fault reaction.

 

This value is t_SLS in the following diagram:

Context

For complete SLS information refer to SLS (Safely Limited Speed).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Milliseconds

Range

[2, 60000]

Default Value

2

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLS_1.TIMETOVELMONITORING

315ch

04h

Unsigned16

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_2.TIMETOVELMONITORING

315dh

04h

Unsigned16

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_3.TIMETOVELMONITORING

315eh

04h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_1.TIMETOVELMONITORING

325ch

04h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_2.TIMETOVELMONITORING

325dh

04h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_3.TIMETOVELMONITORING

325eh

04h

Unsigned16

-

-

Read/Write

No